AXIS#.MOTOR.TYPE

Description

AXIS#.MOTOR.TYPE sets the motor type and the torque control algorithm for the motor. The following table provides the motor types:

AXIS#.MOTOR.TYPE Motor and Control Type
0 Rotary surface permanent magnet motor
2 Induction motor with V/Hz open loop control
4 Induction motor with closed loop control
6 Rotary interior permanent magnet motor
10 Rotary Surface Permanent Magnet (SPM) motor with sensorless control

Each motor type has a set of parameters that must be configured either through automatically setting them to values in motor memory (when AXIS#.MOTOR.AUTOSET = 1) or through manual user settings. The list of required parameters are reported by AXIS#.SETUPREQLIST which updates when the motor type changes. When any of the required parameters are not configured, the drive reports F5005 (Drive motor parameters setup incomplete) on the axis.

The following parameters are required for rotary surface permanent magnet motors (AXIS#.MOTOR.TYPE = 0 or 10):

The following parameters are required for linear SPM motors (AXIS#.MOTOR.TYPE = 1):

The following parameters are required for induction motors with open loop V/f control (AXIS#.MOTOR.TYPE = 2):

The following parameters are required for induction motors with closed loop control (AXIS#.MOTOR.TYPE = 4):

The following parameters are required for rotary interior permanent magnet motors (AXIS#.MOTOR.TYPE = 6):

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000
Feature change 02-01-01-000 Added type 1 for linear SPM.
Feature change 02-06-01-000 Added type 10 for rotary SPM with sensorless control.

General Information

Type

Read/Write

Units

N/A

Range

0, 1, 2, 4, 6, 10
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
AXIS1.MOTOR.TYPE

500bh

04h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.TYPE

510bh

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TYPE

6220

184C

Unsigned8

Read Only

-

AXIS2.MOTOR.TYPE

71756

1184

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TYPE

6220

Unsigned8

Read Only

-